Remote Access via Web Browser

N5185A and N5186A allow you to connect to your signal generator instrument remotely via a Web browser. You can access the instrument from a Web browser using either the hostname or IP address of your instrument.

By default, the remote access via a Web browser is enabled for your instrument. You can choose to enable/disable this access using System Menu (triple bar icon) > Settings (gear icon) > Preferences > Allow Remote Browser Access.

When you remotely access your instrument via a Web browser, the Web UI Home page (shown below) is displayed.

The following information is accessible from the Web UI Home page.

Feature Description Accessible from Requires Login
Home

Displays the following information for your instrument:

  • Instrument Information including Model number, Serial number, Firmware revision, Internal versions, and Description

  • Visa Instrument Address including HiSLIP LAN protocol, VXI11 LAN protocol, TCP/IP SOCKET protocol, GPIB, and USB

  • LAN Details including Hostname, IPv4 address, IPv6 address, and Ethernet (MAC) address

Side navigation bar No
Help ("?" icon) Displays instrument's help documentation. Right side of header No
Log in (user icon) Prompts login and allows for password changing. See Authentication and Change Password to know more. Right side of header No
Control Instrument

Allows you to control your instrument remotely by launching the instrument software GUI in the browser. You must first log in to control the instrument. See Authentication to know more.

You can return from controlling the instrument to the Web UI Home page via Web UI Home in the instrument’s System menu.

Side navigation bar Yes
Reports Aids in procurement of reports intended for Keysight Support Engineers to assist in the diagnosis of undesirable instrument behaviors. See Service menu > Report Generation. Side navigation bar Yes
Update Firmware

Allows uploading a .ctp file via your browser and then using this file to update the firmware of the instrument.

You can upload the .ctp file from:

  • the remote PC to the instrument via your browser.

  • USB - Detects attached USB drives, searching the root of the drives for files with a .ctp extension.

Side navigation bar Yes
Logging Allows configuration of log files intended for Keysight Support Engineers to assist in diagnosis of undesirable instrument behaviors. See Service menu > Logging. Side navigation bar Yes

Authentication

To control the instrument remotely using a Web browser, you first need to log in. Login sessions are valid for 100 days, until the password is changed, or until manually logged out.

The default password is "Keysight". It is recommended to change this as early as possible.

This remote browser password is separate from the Windows password on the instrument.

Change Password

No SCPI, GUI only

Allows you to change the password for accessing the instrument remotely via a Web browser.

The password can be changed from any logged in remote browser, or directly from the instrument’s front panel in the Settings menu, under Preferences.

Changing the password manually or via Restore System Settings will log out all existing Web UI remote browser sessions .

Password requirements:

Preset

This is unaffected by a Preset but is set to "Keysight" on a "Restore System Settings to Default Values."

State Saved

Persistent, survives preset and power cycle but not saved in the instrument state.